• ADP5063 powerup state and D

    Greetings,

    I'm facing a little mystery (or simply confusion) in using the ADP5063.  I've got a circuit that amounts to little more than an ADP5063 breakout, while having the chip's output (ISO SX pins) feeding a 3.3V buck/boost.  The ADP5063…

  • ADP5063 and battery charge level

    The ADP5063 "hides" the battery voltage (VBAT_SNS) from the system when charging is happening, presenting a constant 3.4 V to the system.  In our application, we would like to display a rough indication of charge progress to the user, and we…

  • ADP5063 LiFePo4 Higher Current Load Routing

    Hi,

    I'm designing a system that can draw more than 4A from a LiFePo4 cell. I want to charge the cell using ADP5063. The datasheet states Continuous Drain Current as 2.1A. So I want to route discharge power around the charger when the system is in discharge…

  • ADP5063 How to configure DIG_IOx as stated in table 49 in datasheet?

    Hi,

    recently I started to integrate ADP5063 to my project. Now I stumble on how to reconfigure the DIG_IOx to another option set. We designed our PCB to use "1001" configuration, especially with the interrup output, but now I found no way to set this…

  • ADP5063: Why LDO did not turn ON when VUSB is plugged in (No Fitted Battery)

    I have off shelve ADP5063 (not factory customised), implemented the standard circuit to PCB with DIG_IO1 tied to HIGH (via 3V3 PSU) and DIG_IO2/3 tied to LOW via 600K internal pulls (which attached to MCU GPIO which depend on 3V3 PSU). This is no charger…

  • RE: 说出您心中的ADI年度“贺岁片”,发帖、跟帖送大奖!(公布获奖名单啦)

    我心中的ADI年度贺岁片——提供电源路径和USB兼容性线性的LIFEPO电池充电器ADP5063

  • ADP5065 for LiFePO4?

    I want to design an efficient LiFePO4 charger and Analog Devices offer the ADP5063 however for a 5V input its efficiency is too low because it is a linear design.  The related part - the ADP5065 is an efficient switch-mode design however the datasheet…

  • ADP5063A - 2 LiFePO4 in Parallel

    Is possible to use ADP5063A to charge 2 LiFePO4 connected in parallel?

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032