Hi Team,
The issue has been resolved. Due to insufficient input capacitor this happened. We have added 47uF capacitor near ADP5056 input pins, it is working properly now.
Hi Team,
The issue has been resolved. Due to insufficient input capacitor this happened. We have added 47uF capacitor near ADP5056 input pins, it is working properly now.
Hi all,
I'm implementing a design utilising the ADP5056 Triple Buck Regulator IC.
So far I've had no issues using the datasheet to design the buck regulators, however I believe the datasheet is missing some information.
Q: What is the gate capacitance…
So far, I tried both: increasing Tx power as far as the peak is not clipped, as well as set the SA to lowest sensitivity before over-loaded; nothing resolves that.
Can the quality of ADP5056 affects the EVM? Previously, I have a defective ADP5056 board…
Hi Cyril,
As you've stated, the ADRV9002 devices requires a specific power-on sequence to avoid undesired power-up currents and subsequent damage to the part. On the evaluation board, we use the ADP5056 to control our power-up sequence. If you take a…
The FMCB board uses lower cost input baluns (i.e. Mini-Circuits TCM1-83x or LTCC balun option) as well as a different power supply distribution circuit based on the ADP5056 and LDO's. Note that FMCB board either comes with AD9986 or AD9988 installed…
Hi Luke,
That light is very dim, so do make certain it's definitely not turning on. If it's not turning on that means that the power domains for the ADRV9002 are not being set to the right level, which would explain your difficulties in connecting to…
Hi, Greetings of the day..
I want do to custom design of ZC706 + ADRV9002EVB boards.
I have doubt on the "Grounds". The main ZC706 board is GND while ADRV9002 is AGND. How can I merge the two grounds? Does that mean can I change AGND to ADRV9002 and also…
Hi Oisin,
Thanks for the reply. We have checked with legacy download option as well. The RED LED turns off but the POWER SUPPLY OK LED, D901, does not Turn ON.
We will continue the checks on ADP5056 as mentioned on the lilnk.
However, I would like to…