• Customer programmable fuses on ADP5053?

    I’m interested in using the factory fuses of the ADP5053. Can you provide me
    with further information/documentation on that topic. Can these fuses be
    programmed only by the Analog Devices  or also by the customer?

     

    The fuses are blown at…

  • RE: Schematic for ADP5053 EVAL Board

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADP505X OVP delay time

    Hello!

     

    Good day. Please be noted that the latch-off protection for short-circuit and overvoltage conditions is optional and is enabled:

    • via I2C (for ADP5050 and ADP5051) or
    • by factory fuse (for ADP5050, ADP5051, ADP5052 and ADP5053).

    ADP5054…

  • RE: BUCK and LDO which are not used in ADP5052 are safely set to disable.

    I recommend using the ADP505x design tool.

    This tool has the ability to disable channels and will suggest an appropriate configuration for the un-used pins.

    Here is the link to the ADP505x design tool.

    ADP505x Buck Regulator Design Tool

    ADP5050, ADP5051…

  • ADP5054 ADISimPower Tool

    Dear Sir:

    I  great need ADP5054 to design my Xilinx FPGA K7 system. ADP5052 does not match my need. can you provide support ADP5054 "ADISimPower" Excel File to me? new "ADP505x_BuckDesigner V1.56" only support ADP5050 to ADP5053 not have ADP5054 select…

  • RE: ADP505X EVM Reference Schematics

    Hi Ranganadh,

    Are you referring to the evaluation board schematics? If yes, these information can be found on the respective product pages.

    Here's the link to the ADP5054 eval board documentation:

    http://www.analog.com/media/en/technical-documentation…

  • ADIsimPower Design Tools Download

    IC                  Design Tool                                                                    Download Tool  URL

    LDOs            ADI Linear Regulator Design Tool and Parametric Search  http://download.analog.com/PMP/ADI_LinearRegulators.zip

    ADP1612     ADP161x Boost Regulator Design Tool http://download.analog.com/PMP/ADP161x_BoostDesigner.zip
    ADP161…

  • ADP5073 shorts when enabled

    Hi,

    We have experienced a series of problems with ADP5073. I hope this could help someone with similar issues.

    The design is same as the application circuit in the datasheet and the design tool, with 12V input and -2V output. Parts are selected from…

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032