Answered and Closed
最近在做ADSP BF707的板子,参考官方开发板ADSP-BF707 EZ-Board的电源设计采用ADP5024为BF707供电。但是我这几天测试发现ADP5024上电后没有输出(三路都没有,其中两路DC一路LDO),使用示波器观察,SW、VOUT、FB以及LDO的输出均没有波形和电压(简单的说就是这块芯片上电没上电都没输出,就是完全没有工作),芯片的使能也都接高电平(5V)了。我焊了两块板子,都没有带负载,都没有工作。请问是否有人遇到了相同的情况,可能是什么原因导致的,还是我哪边出了问题,求解…
Hello, I am having an issue with the switching outputs on a new board with ADP5024.
Expected:
VOUT2 =1.8V
SW2 switches from 0~5V (VSYS) at 36% duty cycle, at 3MHz.
Actual:
VOUT1 ~100mV
SW2 switches from -1~4.5V at 20% duty cycle, at 1.5MHz
My schematic…
我们正在开发一款手持设备用到了ADP5024芯片,现在碰到的现象是上电之后芯片好像就进入到低输入电压锁定状态,BUCK输出对地基本上能测到内部的PULL-DOWN电阻,等VIN放电结束后VOUT对地电阻又恢复高阻状态。
从DATASHEET来看,即使UVLO保护后,当VIN达到UVLO以上输出应该恢复正常才对。更何况我们的VIN上电波形是很好的上升波形,好像不应该会锁定才对。
另外Table 2里的UVLOvin1rise UVLOvin1fall UVLOvin1rise UVLOvin1fall…
Hello,
I was unable to find an answer to this in the datasheet... how should I connect the following ADP5024 pins if I do not want to use the second Buck regulator?
VIN2, VOUT2, SW2, FB2, PGND2
Obviously EN2 will be connected to ground in this case…
The ADP5024 datasheet lists these variants but shows nothing different between the two.
Hi
For our application we want to use yours ADP5024 and generate delay Between BUCK1 and BUCK2 Enable pin's.
As mentioned in the data sheet those pins are active logic level high with Vih of min 1.1v.
Your ADP5134 has the feature of precision enable…
LTM8045 |
LTM8049 |
LTM4651 |
LTM4661 |
LTM4686 |
LTM4676 |
LTM4686-1 |
LTM4676A |
LTM4675 |
LTM4677 |
LTM4678 |
LTM8062 |
LTM8061 |
LTM8052 |
LTM8026 |
LTM8056 |
LTM8064 |
LTM8054 |
LTM8055 |
LTM4600 |
LTM4600HV |
LTM4608A |
LTM4604A |
LTM8032 |
IC Design Tool Download Tool URL
LDOs ADI Linear Regulator Design Tool and Parametric Search http://download.analog.com/PMP/ADI_LinearRegulators.zip
ADP1612 ADP161x Boost Regulator Design Tool http://download.analog.com/PMP/ADP161x_BoostDesigner.zip
AD…
针对Altera公司的系列产品的集成式电源解决方案下载 by ADIForum
附件的产品资料是咱们针对Altera公司的Cyclone V (GX/SX)、Stratix IV、Stratix V和Arria V 系列产品的集成式电源解决方案,欢迎下载(有分别针对Altera各个型号产品的详细电路原理图、主要的器件参数设置建议,等等,很给力哦)。
RE: 针对Altera公司的系…