• Interfacing a low-side Mosfet on a 3,3V DSP

    Hi all,

    I need to interface a low side mosfet on a DSP, powered at 3,3V.

    The maximum switching frequency in not so high (300Hz) and the duty cycle can vary between 10:90%.

    The source/sync current available from the DSP is sufficient to turn-on/off…

  • MOSFET Driver OTW terminal Abs Max

    Hi

    I would like to know absolute maximum voltage of ADP3625's OTWb terminal.

    Could I have your help?

    Regards

    moto

    ADP3625,ADP3624,ADP3625,ADO3633,ADO3634,ADO3635

    ADP3629,ADP3630,ADP3631