The datasheet for the ADP3624 says that it can use a supply voltage from 4.5V-18V. The peak output current is only spec'ed for a Vdd of 12V and there are no plots of output current vs Vdd. I see that the rise/fall times and propagation delays would…
I developed a RC speed control for DC motors. It took me about 2 years to get it finished and recently it has been published in Elektor 2014 7/8 p104. The PWM pulses are generated by a microchip PIC12F1840 and directly connected to both input of the ADP3624…
Hi Andrej,
I wonder if the driver ADP3624 has rise/fall time comparable with the pulse width: the specs put these times between 10 and 25 ns. Is it not affecting the modulation?
Hi
I would like to know absolute maximum voltage of ADP3625's OTWb terminal.
Could I have your help?
Regards
moto
ADP3625,ADP3624,ADP3625,ADO3633,ADO3634,ADO3635
ADP3629,ADP3630,ADP3631