Hi all,
The data sheet sheet for the ADP3339 states the the values for the divider resistors, R1 and R2 are chosen to produce a temperature stable output.
Should I not place several ADP3339's in parallel for this reason?
The data sheet also says…
Hi,
In the evaluation board for AD9522, separate power supplies are used for Vs and Vcp.
Is it mandatory?
Can I power both the supplies from a single LDO - ADP3339.
Regards,
Vishnu R.
Hi rrosario ,
I am going ahead with ADP3339 for my design.
I am using one ADP3339 / 4 DDS(AD9959) chips.
Thank you,
Prakash
Hi Ajith,
What you are seeing at the output makes sense, with an input voltage of only 5V, you are operating in the dropout region and the highest voltage level you can get at the output would be 5V minus the dropout voltage(voltage drop in the pass…
I assembled the circuit that was referring to the Figure5 in the AN-934 in order to make the operation test of the AD8336.
In order to operate the AD8336 by itself, we have entered a 250mVp-p sine wave.
When I set GNEG=0.75V and GPOS=1.5V, output signal…
How are things going? We have had to delay our FAQ on a linear regulator design for the ADIS16375, but I wanted to offer some starting points, in case you are going to do this yourself:
Hello,
The user guide can be found at the following link:
Evaluating the AD8283 and AD8285 Evaluation Boards [Analog Devices Wiki]
I have attached the schematic files for the board.
Please let me know if you need anything else.
Thanks!
Kris