Hi,
We are using the ADP3338 and ADP3333 LDOs extensively in our designs.
They are showing Note Recommended for New Designs in the webpage.
Please suggest an exact replacement for these parts (PIN to PIN compatible).
Regards,
Vishnu R.
Hi,
We are using the ADP3338 and ADP3333 LDOs extensively in our designs.
They are showing Note Recommended for New Designs in the webpage.
Please suggest an exact replacement for these parts (PIN to PIN compatible).
Regards,
Vishnu R.
Hello
The ADP3338 is marked "not recommended for new designs" What is the replacement?
https://www.analog.com/en/products/adp3338.html#product-overview
I need to obtain 250mA 2.5V from a 3.3V supply.
We used ADP3338 in in a radiation testing…
我也有这个问题!我买了200颗,目前用了将近90颗,有30++颗出现这问题,里头出现这个问题时候会导致我的ADC出现极大的噪音。请问有什么办法解决?为何会出现这问题?
I'm designing a system for a car with two use cases. In normal operation, the system is powered by the 12V car battery, which is regulated to 5.6V by a buck-boost regulator and then to 5V by the ADP3338. When the system is outside of the car, however…
Hi,ADI Expert
I use the low cost LDO adp3338-5 as the digital power regulator for my design.but now i am confused with the one of its features.I quoted the feature here-- 'Ultralow dropout voltage: 190 mV (typ) @ 1 A'.In my design,i supply adp3338-5…
Hi !
I would be interested in what happens to an ADAU1466 if it overheats, to compare that to the strange behaviour that I am currently experiencing.
In the current revision of my DSP board, I am still using the same supply scheme as on the eval board;…
那么影响最大的是ESR?其他因素随温度怎么变化呢?
目前,我用的主要是LDO ADP124、ADP125、ADP3338,没有找到ADI产品中合适的DCDC
Hi,
Please refer below expert comment for unused pins at ez.analog.com/.../17677
DE_IN,DCLK_IN can be weakly pulled low.
Output port pins can be left float open or floating
Input pixel ports can be left floating
Note: There are specific layout guide lines…
Hi Prakash BJ,
The AVDD and DVDD supply pins of the AD9959 draws a maximum of 325mA when all channels are turned on.
The 800mA maximum output current of the ADM7160 can only supply up to two DDS chips.
There are higher current output LDOs such as the…