Hello,
Using 5V instead of 6V to power the board should not affect the measurement, but it is still recommended to use the board as specified.
Looking at the schematic for the board found here it can be seen that the 6V voltage is being regulated to 5V…
I need to drop down from a higher voltage than the venerable ADP3336 can handle and so I'm looking at the ADP7142. It's only rated for 200ma of current though compared to the 800ma for the 3336 but I think that's still enough for the 1701. …
最近做项目,使用单片机的A/D采样,电源是ADP2300接ADP3336转3.3V,如果ADP2300的输出纹波可以很好的控制,就没必要再加个ADP3336了,所以想咨询下开关电源后面加LC滤波器降低纹波方面的文档或资料,
在AN-1141文档中,
未看到“当输出端使用两级滤波器时(第一级是LC滤波器,第二级是磁珠加去耦电容)”,相关的计算方法资料,
可否提供相关资料,因为以后的产品将要做成电池供电的,所以不想使用LDO了,万分感谢。
AD's eval board uses not merely a garden variety 3.3V regulator to power the -1701, but a ADP3336 low-noise linear regulator. Apparently they felt that low power supply noise would show off the -1701 with best advantage. It will be interesting…
Sorry, just a follow up question... The linear regulator ADP3336 has quite low voltage drop. So is there any difference in the strength of noise filtering, if I apply say 3.7v on its input, or 5v? Or the noise reduction is independent of the input voltage…
I finally figured it out!!
The regulator was NOT the problem. We ordered regulators as well as a whole new dev kit (hoping the regulator would fix it so we could return the new dev kit) I replaced the regulator and nothing changed. I then decided to pull…
Thanks for doing this experiment, Bob. I don't have a lot of in-depth knowledge of LDOs, but I know enough to be able to agree with your assessment.
Skfir, another option if you are really planning on "retiring" the evaluation board would be to lift…
Hello,
I am very concerned with low frequency noise in Sigma DSP processors. I have tried two different eval boards, the latest one is EVAL 1701. I am measuring 1/f noise that is several microvolts/rtHz (@10 Hz) . I am wondering if you can tell me if…