• RE: What is the output current of ADP3335 MSOP ?

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • What is the power up sequence of AD6633 core and I/O?

    the program and other configuration are correct, but there is no current
    output, should it be the power up sequence problem?

     

    The power up sequence is very important. If you power up VI/O 3.3V only and get
    1A current, it proved there is EOS issue…

  • RE: 8MSOP infomation

    Hi,

    Only the LFCSP package of ADP3335 has the exposed pad at the bottom side which should be electrically common with the input pins (pin 7 and 8) for better thermal performance.

    The 8MSOP package does NOT have an exposed pad at the bottom side of the chip…

  • RE: ADV7511

    THanks, I'll discuss with the customer and suggest ADV7511+ADP3335.

    BR Patrik

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • ADI芯片辨识、型号查找

    看看截图:

  • 【在线研讨会回顾】软件无线电技术

    咱们专家在媒体论坛中举办了“集成式软件定义无线电”的技术讲座,介绍了将RF到基带的高速模拟信号链与FPGA数字信号处理相结合,可用于无线通信。话题涉及高速模拟信号链、直接变频无线电架构、高速数据转换器接口以及软件定义无线电中的FPGA数字信号处理。演示使用新一代的模拟器件高速数据转换器、RF和时钟器件以及Xilinx Zynq-7000 SoC。其它话题包括调制器/解调器导致的系统问题,特别是温度和频率变化造成的影响。探讨可以减少这类问题影响的工厂和现场算法,尤其是一劳永逸的工厂预制算法…

  • 软件无线电技术百问百答

    软件无线电技术百问百答 by ADIForum

    咱们专家在媒体论坛中举办了“集成式软件定义无线电”的技术讲座,介绍了将RF到基带的高速模拟信号链与FPGA数字信号处理相结合,可用于无线通信。话题涉及高速模拟信号链、直接变频无线电架构、高速数据转换器接口以及软件定义无线电中的FPGA数字信号处理。演示使用新一代的模拟器件高速数据转换器、RF和时钟器件以及Xilinx Zynq-7000 SoC。其它话题包括调制器/解调器导致的系统问题,特别是温度和频率变化造成的影响。探讨可以减少这类问题影响的工厂和现场算法…

  • 工程师百问百答系列之——软件无线电

    上个月,咱们亚洲技术支持中心的同事在媒体网站上举办了“集成式软件无线电”的主题研讨会。软件定义无线电,这个很“高富帅”的主题很是吸引了大家的关注,这里整理出有代表性的技术问答与大家分享。也欢迎大家就软件无线电相关话题提出您的问题哦(咱们亚洲技术支持中心的专家论坛坐镇支持哟)^_^

    本研讨会介绍将RF到基带的高速模拟信号链与FPGA数字信号处理相结合,可用于无线通信。话题涉及高速模拟信号链、直接变频无线电架构、高速数据转换器接口以及软件定义无线电中的FPGA数字信号处理。演示使用新一代的模拟器件高速数据转换器…