• ADP3338 and ADP3333 replacement for NRND

    Hi,

    We are using the ADP3338 and ADP3333 LDOs extensively in our designs.
    They are showing Note Recommended for New Designs in the webpage.
    Please suggest an exact replacement for these parts (PIN to PIN compatible).

    Regards,
    Vishnu R.

  • RE: Does adv7513 support 720p30 YCbCr4:2:2 input format and convert to 720p60 output format?

    Hi,

     Could you please crosscheck your schematic under 6318.ADV7511W_Eval_Sch_revA.pdf

     Please let us know your Rx ? ADV7513 is HDMI transmitter and it does not have test pattern generator.But HDMI Receivers ADV7611/ADV7619/ ADV7612 with ADV7511 HDMI transmitter…

  • RE: ADV7513 HDMI 0x41 bit6 is failed to set bit

    Hi,

    Could you please crosscheck your schematic here 6318.ADV7511W_Eval_Sch_revA.pdf

    Also make sure again with HPD is high, check 0x42[6]
    or
    override by setting 0xD6[7:6] = 11

    Please note that normally we recommend 5 ms wait after full power up sequence before…

  • ADuCM350 FAQ Debug

    Q: How do I load a *.hex file to the ADuCM350?


    A: When code is compiled and built, EWARM will produce an output file. This output file can be a number of types (e.g. *.out, *.hex, *.bin; the desired type is specified in the project options). The…

  • AD9880/AD9380/AD9381/AD9398/AD9393 Design Support Files

    Attached and linked are several files supporting the development of systems using the AD9880, AD9380, AD9381, AD9398, and AD9393 video Rx products.

    File Content
    PRODUCT SUPPORT
    AD9880 Product Page Link to AD9880 Product Webpage
    AD9380 Product…
  • ADI芯片辨识、型号查找

    看看截图:

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • ADV7510 Design Support Files

    Attached and linked are files supporting the development of systems using the ADV7510 HDMI Transmitter.

    We recommend that, if you download and use this document, you subscribe to email notifications for either the entire forum or at least this FAQ…

  • 【在线研讨会回顾】软件无线电技术

    咱们专家在媒体论坛中举办了“集成式软件定义无线电”的技术讲座,介绍了将RF到基带的高速模拟信号链与FPGA数字信号处理相结合,可用于无线通信。话题涉及高速模拟信号链、直接变频无线电架构、高速数据转换器接口以及软件定义无线电中的FPGA数字信号处理。演示使用新一代的模拟器件高速数据转换器、RF和时钟器件以及Xilinx Zynq-7000 SoC。其它话题包括调制器/解调器导致的系统问题,特别是温度和频率变化造成的影响。探讨可以减少这类问题影响的工厂和现场算法,尤其是一劳永逸的工厂预制算法…

  • 软件无线电技术百问百答

    软件无线电技术百问百答 by ADIForum

    咱们专家在媒体论坛中举办了“集成式软件定义无线电”的技术讲座,介绍了将RF到基带的高速模拟信号链与FPGA数字信号处理相结合,可用于无线通信。话题涉及高速模拟信号链、直接变频无线电架构、高速数据转换器接口以及软件定义无线电中的FPGA数字信号处理。演示使用新一代的模拟器件高速数据转换器、RF和时钟器件以及Xilinx Zynq-7000 SoC。其它话题包括调制器/解调器导致的系统问题,特别是温度和频率变化造成的影响。探讨可以减少这类问题影响的工厂和现场算法…