• ADP3331 Feedback Voltage

    Hi;
    I have used a large number (+10) of ADP3331 in a precision instrument circuit to generate voltages of 1.8, 3.3 and 5V.
    In this circuit, I have used the values of the resistors in Table 1 (page 7 of the datasheet). But the feedback voltage is 0…
  • Feedback voltage of ADP3331

    Hi;

    I have used a large number of ADP3331 (+10) in a precision instrument circuit to generate voltages of 1.8, 3.3 and 5 volts.
    In this circuit, I have used the values of the resistors in Table 1 (page 7 of the datasheet). But the feedback voltage is 0…

  • RE: ADP3331 problem

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Part ADP3331ARTZ-REEL7 is identified as NRND and we had selected this part to use in our new product. Can you please suggest any form fit function replacement for this part

    Hi,

    ADP7118 will be a good replacement part. It has the same output current capability (200mA) and package option (TSOT) when compared to ADP3331.

    Regards,

    Errgy

  • RE: ADF4158 PLL strange 'moving' spurs

    For the reference I'm using a 10 MHz TCXO from Connor-Winfield (D75A). It has a LVCMOS output with about 2.5ns/v slew rate but harmonics every 10 MHz up to GHz ! The design allows an external reference to be used via a splitter between the TCXO which…

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • RE: User Guide of ADF4157 EVB

    Hi Alex,

    I've attached the ADF4157 Eval Board user guide (this should come on the CD). The board uses a parallel port interface but we have included a USB

    adaptor board in all new eval board kits now so you can communicate with this board via USB…

  • RE: AD9528 jitter question

    Chapter 9 Hardware Design Techniques F.pdfHi XY,

    let me respond to your questions:

    If we use Buffer Mode, Output Additive Jitter is about 140fs. so total rms jitter for AFE ADC clocks should be roots.quare(100*100+140*140+54*54) = 180.3fs rms. Is my perception…

  • ADI芯片辨识、型号查找

    看看截图: