• ADP3330: Reverse current

    In the datasheet of ADP3330 there is no indication what is allowed for reverse
    voltage, i.e. if the output voltage is greater than the input voltage(in case
    input power is disconnected and the output capacitor still has voltage). Is it
  • ADP3330: max reverse voltage

    I would like to know what the max. reverse voltage is on your
    ADP3330-3.3 (voltage on output if input is GND)?

     

    Here are the results that you've requested concerning what the max. reverse
    voltage is on
    ADP3330-3.3 (voltage on…
  • RE: ADM2487E: D1/D2 pin

    Hello,

    Thank you for your reply.

    I am using the transformer of Murata.

    Parts#: 782482/33VC

    A primary voltage of the transformer is 3.3V.

    And, I am using the ADP3330.

    The difference with Figure34 in the datasheet is Schottky diode.

    I am using Schottky…

  • RE: AD7190 with instrumentation amplifier

    Hi Dogan,

    your have a 10 kg, 2mV/V loadcell. Is the excitation voltage +5V. So, the total output is 10 mV for a 10 kg weight and there is a change of 1 mV for a 1Kg weight change. To achieve 0.05 grams of resolution, the ADC/PGA needs a p-p noise of…

  • AD7709: FAQs

    the DS recommends (p. 25 of rev0) 10uF tantalum // 100nF ceramic. For
    availability, reliability  and size reasons I would like to avoid tantalum.
    What do you think of a 10uF X5R ceramic instead of the recommended combination?
    What if I add a maybe…

  • RE: 模拟对话 2007年第41卷第1期

    By Colm Slattery [colm.slattery@analog.com]

     

    引言

    电力产业的快速发展推动全世界加强现有电力网的传输和配电并且建设新的变电站。微处理器技术的进步和技术支持人员成本的增加是电力公司使用高精度集成自动化系统设计新的自动高压变电站的主要推动力。

    按照电压高低,变电站可以分为两类:高压变电站包括500 kV,330kV和一些220 kV变电站;而220 kV终端变电站、110 kV和35 kV变电站则归为中、低压变电站。高压(传输)变电站是大型户外站…

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032