• ADP2387 vs ADP2389

    Search in electronics distribution led me to your part ADP2387 (my application needs 12V in, 8.5V/5.5A out adjustable high efficiency sw regulator with programmable current limt), but when I do same search on your website your ADIsimPower tool points me…

  • ADP2389 Output Voltage

    Hi,

    I would like to use ADP2389.

    So, I have a question.

    #1  When I used ADP2389, when the load was changed from 0 to 9 A, the output voltage fluctuated by about 10 mV.

          Is this characteristic of the IC?

          The conditions of the regulator are as…

  • About ADP2389  Inductor&capacitor

    Hi,

    I would like to use ADP2389.

    So, I used "ADP2389/90 BuckDesigner Tool.

    However, a problem occurred.

    When setting under the following conditions, the values of inductor and capacitor differed between my calculation and tool.

    ------------…

  • About ADP2389 Accuracy and minus current

    Hi, 

    I would like to use ADP2389.

    So, I have two questions.

    #1  When RILIM = 59 kΩ, the peak current is stated as 15 ~ 18.6 A. (From data sheet)
        Is this variation in output peak current equivalent (about ± 10.7%) even if the resistance value is changed…

  • RE: Maximum  Vout spec of ADP2389/90

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • Schematic for EVAL-ADP2389?

    Is there a schematic available for EVAL-ADP2389?

    Thank you.

    -Dan

  • Absolute maximum rated current value of ADP 2389

    Hi,

    I would like to use ADP2389.

    So, I have a question.

    Current limit can be set with R (ILIM), but what is the maximum current flowing capacity possible?

    Best Regards,

    Yuya

  • ADIsimPower Design Tools Download

    IC                  Design Tool                                                                    Download Tool  URL

    LDOs            ADI Linear Regulator Design Tool and Parametric Search  http://download.analog.com/PMP/ADI_LinearRegulators.zip

    ADP1612     ADP161x Boost Regulator Design Tool http://download.analog.com/PMP/ADP161x_BoostDesigner.zip
    ADP161…

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032