Hi
I have a question ADP2360.
1.Where is Iq measuring? Is there material of a measuring circuit?
2.Do you have a parameter leakage current to Vin Pin? I want to know leakage current to Vin Pin when both EN is ON and OFF.
Best Regards
HOD
Is CSS(for soft start capacitor) is implemented this bord?
If implemented, I want to know Value .
Hello,
in the datasheet of ADP2360 it is written "the max output current is slightly less than half of peak current IPEAK(through inductor)".
When I check the specs at p. 3 I see I peak is >=126mA (for 0 Ohm), whereas by table 5 at p.12 140mA…
hi
i want to use ADP2360 as a current source in my design. so i connected FB pin to a current shunt resistor .
i intend to get 20ma current over temprature range -40 to 85 .
ADP2360 has an internal 0.8v internal reference voltage and i am worry about drift…
Can I get fig19 detail data?
(I will use this device 41V±4V and 27V±2.7V)
Hi,
Any recommendations about selecting the bottom feedback resistor?
In the datasheet a use case of 115K ohm is shown, but it fits for 3.3V.
I need to produce output voltages of 12V up to 33V.
Thanks,
Kobi
I'm designing a board which will be powered from loop-powered system with 24v/3.2mA input.
I want to convert it to 3.3V/12mA output.
So i want to use adp2360 as dc-dc converter but the problem is in LTSpice the minimum input current from supply…
additional info.
Customer have to use external regulator ADP2360 because of high consumption os scheme. Censor consumes 10 mA peak current every second (0.8 Hz), to compensate this, customer added three big capacitors to input of adp2360.
Hi Rainier,
Yes, the voltage regulator is still working properly and there is no short between -LOOP and COM pins. Thus I'm unable to conclude what might have gone wrong. I will wait to receive new set of ICs and get back to you on this.
Thanks…
好久不见的参考设计终于上新啦!
主题:智能温度变送器
免费下载请点击:http://h.analog.com/CN-REF-STTff?ADICID=SOME_CN_P1659
智能温度变送器评估套件具有高精度、信号隔离、LCD显示、支持HART协议、环路供电、接口保护等特点,此平台主要基于ADI公司的带自校验功能的多通道ADC和EPSON公司的超低功耗16位MCU实现。本设计主IC采用了ADC7124-4,它内部集成了24位∑-△ADC,缓冲器和PGA(可编程增益放大器)。该变送器能将温度…