在使用ADP2323设计中,需求是12V输入5V@1A 和3.3V@2A 输出,完全按照 ADP232x Buck Regulator Design Tool 进行硬件设计,但实际调试过程中5块板子只有一块3.3V输出正常,现象是空载的时候3.3V是正常的,一旦FPGA加载程序,电压就掉到2.3V附近,请AD工程师指导一下调试思路,谢谢
Apart from pre-warming this part at 125 degrees for 24 hours to remove any moisture does anyone have any recommendations to solder this chip onto a board ?
I have allowed a 3 mm plated through hole to allow soldering onto the E-pad but the amount of…
IC Design Tool Download Tool URL
LDOs ADI Linear Regulator Design Tool and Parametric Search http://download.analog.com/PMP/ADI_LinearRegulators.zip
ADP1612 ADP161x Boost Regulator Design Tool http://download.analog.com/PMP/ADP161x_BoostDesigner.zip
ADP161…
C112, C117 and C120 perform the large load for the output of the ADP2323. During soft start, it requires large input current to charge those capacitors to Vout within the soft start time. If the soft start time is too short, the charging current may trigger…
Apart from pre-warming this part at 125 degrees for 24 hours to remove any moisture does anyone have any recommendations to solder this chip onto a board ?
I have allowed a 3 mm plated through hole to allow soldering onto the E-pad but the amount of copper…
我们现在提供的是双通道输出的降压型DC-DC芯片,如ADP2323. 没有您提到的降压模块产品。
如果对ADP2323感兴趣,可以登录ADI官网查看相关数据手册以及资料。
Hi LucaV,
The reason I take ADP1864 and the power sequencing control as a design reference is that its function and performance have been proven in ADSP-2148x EZ board. It is the first time for me to use switching regulator in PCB design. Because of…
Hi Ranganadh K,
Your operating currents across all rails are too high for the chip to handle simultaneously, and this will cause the die temperature to increase, and the part will go into thermal shutdown. Are these your max currents? I suggest that…
"Just to give you an idea of the performance level you can achieve directly from a switching regulator, look at the attached example, and I will be posting one based on the ADP2323 soon"