• ADP2302 max vout

    Hello,

    Uber simple question regarding ADP2302. What is the actual voltage output range when Vin is 12 VDC?

    Looking over the datasheet on page 17, it seems to suggest that Vout can be up to 15 VDC. However, all of the example schematics seem to have max…

  • Best way to apply output voltage to an unpowered step-down converter (like ADP2302)

    Dear support,

    I have a use case similar to the application note from TI here: https://www.ti.com/lit/an/slyt689/slyt689.pdf

    I want to apply external 5V which is on the output side of a step-down converter like the ADP2302. But the IC itself is not powered…

  • ADP2302

    有人遇到稳压芯片ADP2302输出电压电流不稳的问题吗?

    我使用ADP2302一段时间,输入12V输出5V,突然就输出不稳定了,

    是与这电感有关吗?

  • ADP2302

    请问,ADP2302的参考电路中的二极管除去会对整个电路有什么影响?还有这个电感必须是功率电感吗?可以用替代品吗?

  • RE: ADP2302的PGOOD引脚的使用

    电感必须是功率电感,选的时候注意一下饱和电流值。

    二极管一定要加,因为ADP2302是异步的,只有上管,没有下管,所以一定要外加二极管的。

  • RE: ADP2302 self-destructs

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADP2302 output noise issue

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADP2302/ADP2303 fails when powered from SLA battery

    Hello All,

    We designed a circuit using ADP2302 to step down the supply voltage from 10-13.5V to 3.3V for the microcontroller and it's peripherals. We followed the reference circuits and layout without dramatic deviations from the original. While testing…

  • RE: ADP2302 do not want to be loaded

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADP2302/ADP2303; 4 layer PCB required?

    Hello all:

    I'm considering revising a buck converter board that I've designed to use the ADP2302/3 devices instead. I've reviewed both the datasheet and the UG-189 eval datasheet (http://www.analog.com/media/cn/technical-documentation/evaluation…