Hi,
I want to know the ADP2119 supply current. I have read the datasheet. I couldnt find it. Can you help me?
Hi,
I want to know the ADP2119 supply current. I have read the datasheet. I couldnt find it. Can you help me?
Hi,
I am using ADP2119-ACPZ-R7 in the following condition; Vin=3.3V, Vout=1.8V. I didn't find recommended inductors in datasheet. Inductor should be 1.5uH but I am not sure DCR, saturation current and DC resistance value . Can you recommend inductor…
Hi,
I am using ADP211-ADJ. I built the circuit given in the datasheet, but I see 3.68V instead of 3.3V in ltspice. Could ltspice be giving wrong results?

主电源为5V,数字和模拟部分也都需要5V,在不使用隔离的情况下,模拟部分的AD7606可以用ADP2119来供电吗?因为是5V输入,5V输出,没有见到这样的实例,有没有用过的朋友给指点一下,效果如何?
Hi all,
I have a question on ADP2119.
Regarding the ouput voltage accuracy of the fixed output version,
Do you have any data on it?
I want to achieve1.0 output voltage within 3 % errors.
So It would be great if the information of internal FB resistors…
Hi Prithvi,
Thank you for your interest in using the ADI parts in your application. May i know why you choose ADP2107 instead of newer, simpler (internally compensated) but cheaper ($1.25 vs $1.5) part like ADP2119? The ADP2107 and ADP2119 were both can…
Please start to check with LTC3307 or ADP2119. https://www.analog.com/en/products/ltc3307a.html or www.analog.com/.../adp2119.html
Other options (copy and paste to browser): here: www.analog.com/.../11491
Dear Team,
Kindly refer to the schematic snapshot below for ADP2119ACPZ-1.2-R7.
We are getting 0.6V at the output of this regulator at inductor L1 even though this is a fixed output voltage regulator. The branding of LFK printed at the regulator confirms…
I am really sorry that this post was not answered. If this becomes an interest again in the near future, you can use a switching regulator, but would want to pay close attention to managing your output ripple and any other noise sources. The ADP2119 might…
Unfortunately we do not currently have a buck-boost that is capable of delivering 1.5A from 1.8V.
It could be done with a boost regulator such as the ADP1614 charging a large enough cap and followed by a buck regulator like the ADP2119.
The only buck…