• ADP196 WLCSP Footprint

    Hi,

    I am just reviewing the footprint my colleague has drawn for the WLCSP package of ADP196. They used a pad diameter of 0.24mm, which is ~20% reduction from the ball diameter. This is consistent with the recommendations of IPC-7351.

    I downloaded the…

  • Paralleling two ADP196

    Hi,

    Can I parallel two ADP196 in order to get more current (4A~5A)?

    Thanks,

    Noam

  • ADP196 replacement for ADP198

    I am designing a small, battery operated device and am using a high-side load switch to isolate the battery during the charge process.  I originally used the ADP198 in the design, but I need greater current capacity.  I used the device in its diode OR-ing…

  • 想问一些关于负载开关的问题

    最近想使用一款负载开关,要求是单通道双向逻辑控制开关。之前选了一个ADP196,但是它不是双向的,有没有用过相关器件的工程师给我推荐一款,谢谢

  • 关于AD7656低电平输出质量差的问题

    大家好,在做好的AD7656的电路板做测试时发现,在上电后AD7656工作之前,AD上输出的低电平波形是比较干净的,但是当给AD7656复位开始工作后,AD输出的低电平波形很差,毛刺很多,但是高电平输出是干净的,请问这是哪里出了问题。

    这是画的电路图的一部分,电源模块没给出。其中模拟地与数字地之间是通过一个磁珠隔离开的。电源用了ADM1185、ADP1613(正负12V)、ADP3303、LM1117、ADP196。

  • 最新中文资料更新20131226