• ADP1829 Dual buck controller with a high side N channel FET

    I would like to use the ADP1829 dual synchronous buck controller with a high
    side N channel FET switching from 120 volts. To do this I intend to use an
    IRS2011 high and low side driver, but it means reconfiguring the high side
    driver of the ADP1829…

  • 重磅推荐!48 款电源参考设计

    ADI 为基于电源的应用开发了一些参考设计,今天为大家推荐其中的 48 款,每款设计均包含仿真、图形和测试数据。 提供文档和文件,可重建设计。 另外,针对某些设计还提供基准测试硬件。需要哪款参考设计,自行拿走~

    ps.这里给出的每款参考设计都是PDF链接,无需注册哦

    再ps.对于这种满屏都是干料的帖子,你还不快快点赞、分享?! 

  • RE: Can I use the ADP1872 to design a bidirectional converter?

    Hello Dhiogo,

    The ADP1872 is not a good choice for a bidirectional converter because it is a current mode part.  It would be better to choose a voltage mode part like the ADP1828 or ADP1829.  We have in fact used these parts for high current DDR termination…

  • RE: 签个到,送您好礼啦!(获奖名单已公布)

    我在常州+新北区三井街道+我是做电源产品开发的,所以最关注电源产品及其IC(如ADP1864,ADP1829、ADP1655等)的的性价比及功能,IC内部的逻辑结构!

  • FAQ: Tips for taking efficiency data

    Attached is documentation on a quick easy way to get accurate efficiency measurements .

    Attachments:
  • ADIsimPower Design Tools Download

    IC                  Design Tool                                                                    Download Tool  URL

    LDOs            ADI Linear Regulator Design Tool and Parametric Search  http://download.analog.com/PMP/ADI_LinearRegulators.zip

    ADP1612     ADP161x Boost Regulator Design Tool http://download.analog.com/PMP/ADP161x_BoostDesigner.zip
    ADP161…

  • AD9523/PCBZ Evaluation Kit Input Voltage and Through Holes

    I would like to test the AD9523 evaluation board inside of a computer case, however running the wall wart power to it is very cumbersome.  6V (or 2.2V and 4V) are not readily available in the case, but, since I'm using a standard computer power supply…

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032