• RE: LDO Regulators in Parallel

    Hi ,ADP1765 Fixed output parallel , how to connect the VADJ ?

  • Paralleling more than two ADP1765

    Hello,

    My application requires very high currents (~20A max peaks) and low noise thus I'm looking at the ADP1765 as the LDOs for the job. I would need to parallel 4 or 5 of them, should I just parallel all of them as indicated for 2 devices in the…

  • RE: ADP1763: Max capacitive load that ADP1763 can support

    Hi Guha,

    It is case to case basis. Stability may be a concern at very high output capacitance. A similar question was posted for ADP1765 a while ago that used LC filter with total 1mF of output capacitance. Result was still acceptable. In your case, you…

  • Noise below 100Hz in ADP1762/ADP1764

    I am trying to determine which ADP1760 series regulator to use. I have a low current requirement (<2A) so it would seem that ADP1762 would be fine.

    However, the ADP1764 and ADP1765 regulators have significantly lower noise below 100Hz than ADP1762…

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032