• ADP1764 EN, PG pin

    Hi,

    I want to know about EN and PG in ADP1764.

    Vin -> 1.2V
    Vout -> 0.925V
    EN -> 3.3V
    PG -> 3.3V Pullup

    I am thinking of configuring ADP1764 as above.

    When I look at the Absolute Maximum Rating Table, I think ADP1764 will work.

    Considering that…

  • Managing Output Voltage ADP1764 LDO with LTC2977

    I need to manage several ADP1764 LDOs using LTC2977 sequencer. Adjusting the output voltage of the ADP1794 can be done with an IDAC, however the LTC2977 has VDAC.

    Can you suggest an easy connection between the LTC2977 and the VADJ pin of the ADP1764?

    1. Enable of ADP1764

      Hi,

      I am using ADP1764 in my design. I want to connect the Enable pin to my controller. Below are the details about Vin, Vout and Enable logic level. Let me know if this works. If not please let me know how I can proceed with implementing this. 

      Vin to…

    2. Noise below 100Hz in ADP1762/ADP1764

      I am trying to determine which ADP1760 series regulator to use. I have a low current requirement (<2A) so it would seem that ADP1762 would be fine.

      However, the ADP1764 and ADP1765 regulators have significantly lower noise below 100Hz than ADP1762…

    3. TAGS LIST: Power Management

      LTM8045
      LTM8049
      LTM4651
      LTM4661
      LTM4686
      LTM4676
      LTM4686-1
      LTM4676A
      LTM4675
      LTM4677
      LTM4678
      LTM8062
      LTM8061
      LTM8052
      LTM8026
      LTM8056
      LTM8064
      LTM8054
      LTM8055
      LTM4600
      LTM4600HV
      LTM4608A
      LTM4604A
      LTM8032