• Looking for PMIC like ADP1707 with tracking

    I'm looking for PMIC like ADP1707 with tracking. As you know, ADP1707 have 50mV(max) dropout voltage, so I want to reduce down dropout voltage to 30mV(max). In conclusion,When input voltage is 0.8V~3.3V, output voltage is 0.8V+30mV ~ 3.3V+30mV.  If…

  • RE: AD9912 power supply

    Saurabh,

    In general I would point you to the ADIsimPower tool for identifying your best options

    Here are a few options for you in the meantime:

    - For the 14.8V to 5V you can use the ADP2370 or the ADP2300 (1/2/3)

    - For the LDO from 5V to 3.3V we have…

  • AD9912 trouble with PLL

    Hello.

    I'm have a trouble with AD9912 DDS.

    AD9912 DDS powers from two sources: +3.3V and +1.8V (I'm use linear stabilisators ADP1707).
    System clock input is KX7-T-40 Mhz, which maximum crystal motional resistance is 50 Ohm.
    PLL Loop Filter is…

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032