• Equivalent to ADP1613 and OP777

    Good afternoon,

    Is it possible to know if the integrated circuits ADP1613 and OP777 have a DIL/DIP package? If not, do they have equivalent ICs in that form?

    Thank you and best regards,

    Alessandro

  • Problem suply with adp1613 5V to +-15V to ADC3023

    Hello
    I have designed the power circuit for the ADA3023 converter that is on page 21 of the data sheet, using an ADP1613 in a SEPIC-Ćuk topology with 5V input and + -15V output. as I see in the data sheet allow an output current of 2A. The problem is…
  • About ADP1613 COMP pin absolute maximum rating

    Hi

    I have a question about COMP pin absolute maximum rating.

    In the datasheet, COMP to GND = 1.0V to 1.6V.

    But I don't know 1V to 1.6V absolute maximum rating. 

    Is the operation range 1V to 1.6V?

    My customer found 2.1V COMP pin voltage in the customer…

  • Boost about ADP1613

    I find this reference designed,there are some form that show the result of the designed.I want to know how you calcurate the parameters. is there a excel or model to help to calcurate the parameters?like the calcurate power of the diodes?

    https://www.analog…

  • Trouble with ADP1613 DC/DC

    I have designed a circuit according to the reference circuit found in the ADP1613 datasheet. Attached is my schematics and PCB.

    Problem is that when i power the circuit, my PSU current-limits even though no load (ive tried bleeder resistors, doesnt work…

  • RE: ADP1613 and ADM7150 layout suggestions

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADP1613 SEPIC - spikes on output

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADP1613, inrush current at inductor

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Elaboration regarding the ADP1613's capacitor equations

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Can you show me how to make an ADP1613 spice model?

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,