FAQ
Hello,
I'm interested in using ADP1607 in a one cell NiMH project. I expect to have 100mA @ 3.3V on ADP1607 output.
When the reverse battery protection is shorted the device is working as expected. When the reverse battery protection (IRF7410) is active…
We got our first samples back that has our device with the ADI regulator (ADP1607ACPZN-R7) on there. We are seeing something that I don't understand and may make this regulator unusable.
We are trying to get an output voltage of 1.875V with a max…
Hi
ADP1607 datasheet say "0.8V to Vout input voltage range"
But when Vin=Vout, it doesn't work. I think.
In other colum, it need reduce diode or cascode FET voltage , I think.
"To use the ADP1607 in the VOUT = 2.5V portion of your application…
Hello,
My name is Meir and I am a DFAE in ADI team at Phoenix Technologies Israel.
Meprolight, one of our customers, is interested in ADP1607 for battery powered application.
Their Input voltage range is: 0.8V-3.3V
Output: 2.5V and 3.3V (depending…
Hi Anita, Just so we are on the same page we are talking about the ADP1607.
I didn't see anything in the datasheet that talks about what happens to the current when Vin > Vout in normal operation.
I will reach out to the product line and get back…