• RE: ADP151 LDO Damage

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADP151 Thermal Resistance

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Use ADP151 in a wired or configuration

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADP7104 and ADP151 input and output Capacitor

    Dear support,

    in my design I use ADP7104 and ADP151 linear regulator.

    In the figure 2 on pag.1 of the ADP7104 datasheet it reports an Electrolytic Capacitor, if I correctly understand,

    but on pag. 17 of the datasheet, it is written that ceramic…

  • RE: 关于ADM7155和ADP151噪声比较的问题

    你好,我再用ADP151 3.3V的LDO时,发现对于非常低频的噪声,LDO的抑制好像没什么效果(0.3Hz的样子,手册上也没有关于10Hz一下的PSRR),这是片子本身的性能吗

  • ADP151 draws high current with output capacitor; outputs +0,2V without

    Hi,

    I designed three ADP151 LDOs (two 2,5V and one 1,8V) into my latest circuit.

    Yesterday I got the PCBs and was suprised in a way.

    All three are drawing too high currents without loads. If I would let them they would draw more than 100mA (I tried…

  • ADP151 for Dual Power Supply

    Dear forum,

    I just wondered if it is possible to use the low noise voltage regulator ADP151 for a dual power supply. I would source -5V to the GND pin and 0V to IN for the negative output, while on the positive side everything 's normal.

    Yours,

  • RE: ADP151ACPZ-1.8 exposed pad connection in adjustable output voltage operation mode

    Hi Osipov-ae,

    Connect the EPAD to the PCB GND where the ADP151 GND pin is also connected.

    Best Regards,
    Alex

  • Power supplies design of AD9208BBPZ-3000

    Hi,

    My customer is designing a power circuit for AD9208BBPZ-3000.

    The recommanded power voltages for AD9208 are shown in the table below.

    However, AD9208 evaluation board schematic in ADI web supplied 1.8V for AVDD2, DRVDD2 and SPIVDD.

      1. Could customer…

  • RE: ADP150 and capacitor choise

    Got it. The selected components are good. It will be better if C3 can parallel with C4. In addition, for the layout of ADP151, please place ADP151 close to the chip need powered. Thank you.