FAQ
I have one through datasheet of ADP124 and it is mentions that "A minimum of 0.70 μF capacitance with an ESR of 1 Ω or less is recommended to ensure the stability" and i need some addition details for power supply application
1) at what…
I've run into a strange problem with an ADP124 3.3V regulator. I have a design that has a 5V rail that is used to power the ADP124 regulator as well as an ADR130 1V Reference. The output of the ADR130 is sent to a MAX5482 Digital pot. The wiper of…
那么影响最大的是ESR?其他因素随温度怎么变化呢?
目前,我用的主要是LDO ADP124、ADP125、ADP3338,没有找到ADI产品中合适的DCDC
Hi Valued User,
Can you send a scope shot when "fault" condition occurs with probes to Vdd, INx, Sx, and Dx of the ADG836L so we can trace what is happening in the device?
What is your power-up sequence?
For the line "Vdd starts to oscillate…
Hi everyone,
I'm designing a circuit with some ADP125 LDOs for the analog supplies. In the abs. max. ratings, there is a requirement for VOUT:
VOUT to GND | -0.3V to VIN
This would clearly indicate that the regulator needs a reverse diode from…
LTM8045 |
LTM8049 |
LTM4651 |
LTM4661 |
LTM4686 |
LTM4676 |
LTM4686-1 |
LTM4676A |
LTM4675 |
LTM4677 |
LTM4678 |
LTM8062 |
LTM8061 |
LTM8052 |
LTM8026 |
LTM8056 |
LTM8064 |
LTM8054 |
LTM8055 |
LTM4600 |
LTM4600HV |
LTM4608A |
LTM4604A |
LTM8032 |
Presenter: Ke Li, System Applications Engineer
The webinar will discuss some of the electronic design challenges with Industrial electromagnetic flowmeters. It will compare conventional analog demodulation with a newer digital oversampling architecture…
揭开高性能多路复用数据采集系统的神秘面纱 by ADI_Amy
高通道密度数据采集系统用于医疗成像、工业过程控制、自动测试设备和40G/100G光通信系统可将众多传感器的信号多路复用至少量ADC,随后依序转换每一通道。 多路复用可让每个系统使用更少的ADC,大幅降低功耗、尺寸和成本。 逐次逼近型ADC——通常根据它们的逐次逼近型寄存器而称它们为SAR ADC——具有低延迟特性,因此适合用于要求对满量程输入阶跃(最差情况)作出快速响应而无任何建立时间问题的多路复用系统。 易于使用的SAR ADC提供低功耗和小尺寸…