• RE: Configuration of the output voltage on the ADP123-EVALZ

    I have found that the problem was in Data Logger (It broke).

  • ADP123 the notation of output voltage accuracy

    I have a question about the ADP123 data sheet.
    I read the datasheet. (Rev. E)

    http://www.analog.com/media/en/technical-documentation/data-sheets/ADP122_123.pdf
    I was strange about the notation of output voltage accuracy.


    The adjustable range of the ADP…

  • RE: BF-548 Power Tracking IC ADP1823

    Hi,

    I didn't understand your point. What is the problem in using ADP123 to generate these voltages.

    Regards,

    Nabeel

  • RE: ADV7612 and ADV7511 reference design questions

    Hello, Guenter!

    Please explain what is the difference between ADV7612 and ADV7511 power supply requirements?

    Why on EVAL-ADV7612-7511 board power supplies for ADV7612 and ADV7511 are also different?

    1). Why for ADV7612 1.8V and 3.3V power supplies…

  • RE: Questions on the ADV7171

    Hello,

    1) There isn't any specification for VAA's noise/ripple characteristics.

    2) Linear / Switcher isn't particularly important but given the relatively low current draw-- something like the ADP123 would probably work well.

    3) I haven…

  • When there is a negetive voltage exist on the output of ADP7142, it will not work.

    Hello everyone,

         There is a problem when I use ADP7142. When I apply a negetive voltage below -0.5V, the LDO will not work. Once the voltage over than -0.5V, the output go back to normal as the curve I captured(the yellow one is a negetive voltage from…

  • TAGS LIST: Power by Linear

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • ADI最新的EM流量计解决方案上线啦

    电磁流量计作为目前使用最为广泛的流量技术之一、液体流量测量中精度最高之一,你了解多少呢?

    先呈上【ADI最新的EM流量计解决方案】下载链接:http://h.analog.com/CN-APM-FLOWMETERff?ADICID=SOME_CN_P1657

    工业电磁流量计系统原理和典型架构

    电磁流量计的工作原理基于法拉第电磁感应定律。当垂直于磁场方向的导体以速度V做切割磁力线的运动时,导体的两端会产生一定的感应电动势E,通过检测该感应电动势的大小来计算液体流速变化。

    电磁流量计的特性包括无压力损耗…