• RE: Wrong LDO output voltage ADP122

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADE9000 shield kit design

    Hello

    you could but you system performances would decrease

    ADuM6404 pin 15 (VISO) - you need 5V because ADP122 will use this value to power ADE9000 with 3.3V. This choise is linked to ADUM high noise at VISO pin compared to ADP.

    As a direct consequence…

  • RE: 2 questions of power for ADN4605

    Hi Kaos,

    1. Pin C24 should connect to the DVcc supply which is 3.3V.

    2. The ADN4605 has four distinct supply pins (actually 5 including ground): VCC, DVCC, VTTI, and VTTO

    VCC, VTTI, VTTO can operate on over a nominal range of 2.5V to 3.3V, where DVCC…

  • RE: ADV7612 and ADV7511 reference design questions

    Hello, Guenter!

    Please explain what is the difference between ADV7612 and ADV7511 power supply requirements?

    Why on EVAL-ADV7612-7511 board power supplies for ADV7612 and ADV7511 are also different?

    1). Why for ADV7612 1.8V and 3.3V power supplies…

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • ADI最新的EM流量计解决方案上线啦

    电磁流量计作为目前使用最为广泛的流量技术之一、液体流量测量中精度最高之一,你了解多少呢?

    先呈上【ADI最新的EM流量计解决方案】下载链接:http://h.analog.com/CN-APM-FLOWMETERff?ADICID=SOME_CN_P1657

    工业电磁流量计系统原理和典型架构

    电磁流量计的工作原理基于法拉第电磁感应定律。当垂直于磁场方向的导体以速度V做切割磁力线的运动时,导体的两端会产生一定的感应电动势E,通过检测该感应电动势的大小来计算液体流速变化。

    电磁流量计的特性包括无压力损耗…