• READ_POUT refresh rate ADP1055

    Hi,

    I 'd like to use the output power metering of the ADP1055.

    About READ_IOUT we can read in the datasheet:

    The READ_IOUT command reports the average output current; this reading is updated every 2.6 ms.

    About READ_VOUT we can read in the datasheet…

  • ADP1055-EVALZ UG-710 input voltage

    Dear all

    I have a question about ADP1055-EVALZ UG-710.

    Can it input -48V negative voltage?

    Most of communication vendors used -48V(input) to 12V(output) module.

    If OK, I think there are some opportunities at communication vendors.

    https://www.analog.com…

  • ADP1055 as dual-phase, interleaved buck converter

    Hello,

    I want to use further buck converter in parallel. The converter are controlled by ADP1055(digital current share function).

    Output power of 3.6KW.

    I have a question about the ADP1055:

    Is it possible to use it as a dual-phase, interleaved buck converter…

  • ADP1055 Active snubber

    I am looking at using the ADP1055 for my phase shifted full bridge converter. Can i get more details about GPIO3 & 4 PWM acting as an active snubber please? Also a schematic of the associated external hardware would be great?

  • Function OC_LV in ADP1055

    Hello,

    i'm using ADP1055 controler for a DC/DC power supply and try to configure the function OC_LV.

    In our configuration the ADP 1055 operates in CCM with manufacturer specific.

    I try to set the IOUT_OC_LV fault at 23V and unfortunatelly in constant…

  • ADP1055 External Synchronization with Spread Spectrum

    Dear Sirs

    I would like to use ADP1055 with external synchronization clock featured spread spectrum modulation.
    For example, LTC6908-1 (Fcenter = 200-400 kHz, ±10% Frequency Spreading).

    But I not sure that ADP1055 can support spread spectrum clock on…

  • RE: ADP1055 EVAL

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • (ADP1046A ADP1055)What is the different between these two device?

    Hi !

    Our customer are using ADP1046A.

    But maybe they will change to ADP1055.

    What is the different between these two device?

    I am reading datasheet now.

    But I could not find anything other than the GPIO difference.

    Best regards

    Kawa

  • RE: Parallel output for ADP1055

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADP1055 PRIMARY FAST OVERCURRENT PROTECTION

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,