Q
Our customer needs to implement programming support of the ADP1051 on theirdevice programmers. To be able to program configuration into EEPROM we need the
EEPROM programming procedure?
Hi Sir
I want to design the ADP1051 as a power module,
can you support the design tool as EXCEL?
thanks
Hi Sir:
Does ADP1051 has OTP function inside that is not triggered by OT_FAULT_LIMIT REG, but by the temperature of its junction?
Hello,
Where can I find design files for the eighth brick reference design based on ADP1050 or ADP1051 or ADP1052?
Is there a demo board for the brick for sale?
Thank you,
Alex.
Sir:
How to export communications spy's data to excel or notepad? or how to get the pmbus log during continuous monitoring?
thanks a lot;
Hi Sir:
1\ In ADP1051's datasheet, page 6, test condition for CS2 current measurement sense accuracy is "4.99 kΩ (0.01%) level shift resistors"; is that a typo? it's impossible to use 0.01% precision resistor in real application, right?…
請設計ADP1051 在音響擴大機上面,約莫1000W
但在輸出電源上需要雙電源並為正/負電 ,不知道有沒有雙電源設計可供參考 ?
Hello, I would like to use two adp1051 in full bridge phase shift topology. According to manual, I can use OUTC to synchronize the other adp1051. But in that case, OUTC becomes useless in term of phase shift for switching the C branch. How can I manage…
Does Gui will surpport the output current doubler solution ? thanks
Dear All:
I Need ADP1051 EVB Board Gerber file P/N:ADP1051-240-EVALZ & ADP1051DC1-EVALZ ,can you provide to em refer. thanks
Best Regards,
Jack