FAQ
The application note AN-1306 is a good guideline for EEPROM programming and factory calibration. Visit the link to see the details:
http://www.analog.com/static/imported-files/application_notes/AN-1306.pdf
The CS1 pin of the ADP1043A, ADP1046A, ADP1050, ADP1051, ADP1055 can not be floating (no resistor is connected between the CS1 pin and ground). there is a tiny source current in this pin. If CS1 pin is floating, the voltage of CS1 pin will be higher than…
In the data sheet of ADP1046A and ADP1050/51/55, the VS- pin (VS3- pin for ADP1046A) voltage should be within -0.3V ~ +0.3V referred to AGND pin. However, since the VS- is the negative remote voltage sense input, the load voltage sense point (remote voltage…
Hi,
Win10系统下,ADP1050-1-2 Evaluation Software显示 “没有注册类”,这个怎么解决啊?
Where can I find a programming procedure to implement EEPROM programming of
ADP1051?
Please see the ADP1050 and ADP1051 EEPROM programming procedure AN-1306.
This document can be found onour website at:
http://www.analog.com/media/en/technical…
Hello, Catur.
For PFC with universal input, you may want to look at ADP1047 and ADP1048. PFC evaluation boards (300W and 600W) are available.
Other PFC controllers can be found here.
About the DC-DC block, you may refer to ADP1046A. Evaluation boards…