• ADP1047 Evaluation GUI Installation

    Hi..While installing ADP1047 Evaluation GUI,it showed some error occurred in installation and says download latest adobe flash player (Installed latest adobe flash player in computer)

  • Questions of ADP1047 testing

    Hi

    Now is testing ADP1047 EVB and its output connect to a DC to DC power board. I have two issues need your support


    1. During the testing, sometimes the ADP1047's inductor current works strange when power on in full load condition. (Seems PFC function…

  • discussions with "Chris" on ADP1047 applications

    This is regarding tons of texts on ADP1047/48 applications: I was expecting an exciting answer from "Chris" who called me last Wednesday. Ended with  a statement to the effect that he would look into the "<50 Hz  zero placement restrictions…

  • RE: ADP1047 Recommended Settings

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADP1047  THD&PF

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADP1047 some questions

    Hi ,

    Got some questions , would you kindly help to reply me ? see the list as below . Thanks

    1. Current sensing ADC of current loop: Clear description, Gain? Whats the level shift current source? ……{page 12, Figure 7}
    2. How to get IL? ……………………………
  • ADP1047 THD問題

    請問 ~ ADP1047 300W evb , 我測試到THD非常高在30W的時候 ~ 大約THD落在50左右

    這樣是正常的嗎 ? 有人說內建的設定檔案是有誤的? 還是誰有正確版的可以分享一下 ?

  • ADP-I2C-USB _USB to I2C Interface Connector

    Where can I get the datasheet of ADP-I2C-USB.

     

    You can refer below link to download it's datasheet.

    http://www.totalphase.com/products/aardvark_i2cspi/
  • Half-bridge dc/dc controller

    I am looking for a Half-Bridge DC/DC Controller for medical application. DC
    input is +360V, output +36V/10A. Isolation transformer should meet medical
    double insulation reguirements. Could you help me with this?

     

    We really do not have…
  • ADP1047, PFC output voltage regulation

    Hi

    I'm working on a PFC input stage built around an ADP1047. The input is 230 volt 50 Hz, the output 385 volt DC and the maximum power

    is supposed to reach 2100 Watt.

    It's working quite nicely up to a power level of about 800 Watt. If the load…