• ADP1046A design question

    Hi Sir,

    Already check all reference design for ADP1046A, I can see the maximum power supply can be reach 600W.

    Please help to make sure the ADP1046A whether cen be meet below request?  Thanks.

    1. Input voltage : 800V DC. Output voltage 200V 3A.

    2. Input…

  • ADP1046A Current Sharing Detail Description

    Hi,

    Several of ADP1046A are planned to be used in parallel for increasing of power supply output current. The ADP1046A current sharing feature can be used for the task. But I can't find any detailed information how to configure the ADP1046A to get shared…

  • ADP1046A-100_EVALZ


    Dear Sir,

    I want to modify the ADP1046A-100_EVALZ to get the 24Vin, 5Vo/6A.

    I change the R10 of main board from 10ohm to 20ohm, and R5/R7/R10 of Daughter card from 11Kohm to 4Kohm, and R1 of Daughter card FROM 27Kohm to 12Kohm.

    And  below is some questions…

  • We need 500W~3000W PFC solution.

    Hi

    We're looking for 500W~3kW PFC solutions, e.g. using Interleave PFC. The target application is UPS and the potential would be 3k units/y. MP will start April 2021.

    Would ADP1046A be available for this ?

    Regards,

    Hiroyuki

  • What is the difference between ADP1043A and ADP1046A

    The package and Pin configuration of ADP1043A and ADP1046 are the same. What is key difference between ADP1043A and ADP1046A?

  • RE: Board Settings for ADP1046A

    I have received the gerber file for ADP1046A from the local analog team and fabricated 5 PCBA for our development and to integrated with our power board. How to program the new ADP1046A IC for default settings and need to change accordingly for my design…

  • How to implement CC mode operation for Battery charger application

    Hi Team,

    I had a look and detail study on ADP1046A and i want to implement in my project for Battery Charger application.

    In datasheet they have explained CC mode operation in pg.no 30 as per below

    In battery charger application, CC mode plays the major…

  • RE: Usage of ACSNS pin on adp1046 LLC Half bridge resonant mode.

    Thanks a lot for the Info.

    I have one more questions.

    I want to use ADP1046A for the battery charge application. Please see the below details for CC mode operation.

    In battery charger application, CC mode plays the major role until it crosses boost…

  • ADP1046A GUI - Register loading

    Hello,

    In setup window of ADP1046A GUI, I changed PWM setting and saved it into my_setting.46r.

    I closed ADP1046A GUI and executed the GUI again. Then I loaded my_setting.46r. But no change in GUI.

    How can I retrieve my own GUI configuration?

    1) I…

  • ADP1046A 600W Phase Shifted Full Bridge Topology Board Availability

    Hi,

    I found Power Reference Design (PRD1404) ADP1046A Wide Input Range, Full Bridge Phase Shifted Topology on ADP1046A Product Page. This document describes 600W Phase Shifted Full Bridge Topology Evaluation Board. So, could this board be purchased?…