• TAGS LIST: Optical

    AD800
    AD803
    AD807
    AD808
    ADN2804
    ADN2805
    ADN2806
    ADN2807
    ADN2811
    ADN2812
    ADN2813
    ADN2814
    ADN2815
    ADN2816
    ADN2817
    ADN2818
    ADN2819
    ADN2855
    ADN2905
    ADN2913
    ADN2915
    ADN2917
    ADL5315
    ADL5317
    LTC5100
  • RE: CN0395 with ADICUP360 demo with 'ADC Data Error' message

    Hello,

    To me it looks like a hardware issue. Which revision of the board are you using? As I recall, on the first revision, the ADN8810 IDAC was always on standby as the SB_N pin was tied to GND instead of VIO. 

    One thing you can try, is to check if there…

  • RE: Using Laser Diode Driver IC (ADN2871) for different polarity  laser

    Dear Nathan,

    Are you interested in ADN8810?

    Please note, ADN8810 could deliver a programmed current to a laser, per its digital interface control.

    Please also note, laser diode optical power output would have aging, temperature,

    and process related…

  • RE: Current stability of ADN2830?

    Hi Luca,

      Thanks for the quick reply.  Seems like ADN8810 could do the trick stability wise, but our diode typically operates around 5V for 100mA.  If I read the ADN8810 spec sheet correctly, the compliance voltage is limited to 2.5V, where the ADN2830…

  • Is ADP2291 working as expected in the datasheet or its examples are fail?

    Hello Everyone,

    Im working on a battery charger circuit. I set completely the figure-22 and the figure-23 in the datasheet. So more than hundred try and later than weeks. The circuits are not working as expected. This part is important "The circuits are…

  • ADI芯片辨识、型号查找

    看看截图: