FAQ
We're using ADN4695E in a point-to-point topology with a 100Ω termination at line end.
ADN4695E datasheet says "Supported bus loads: 30 Ω to 55 Ω".
But we're not sure if it's for a multi-point bus, as AD4695E is suitable…
Hello
Our customer will use ADN4695 and evaluates this.
Then , the measured differential output voltage of driver is about 1.6Vpeak to peak (Y-Z) at 50ohm load ( using two 100 ohm termination).
The customer asks us if value of 1.6Vpeak to peak is abnormal…
We're using ADN4695E in a point-to-point topology with a 100Ω termination at line end.
ADN4695E datasheet says "Supported bus loads: 30 Ω to 55 Ω".
But we're not sure if it's for a multi-point bus, as AD4695E is suitable for, or if it…
Q: Are simulation models available for M-LVDS transceivers?
A: Yes, IBIS models are available through the products pages, the topic page or the direct link provided below:
Download ADN469xE IBIS Models:
Q: Do you have an M-LVDS evaluation board?
A:
There are two high performance evaluation boards available, the only ones available on the market. Competitor boards are not optimized for high speed measurements.
MLVDS Half Duplex High Speed Evaluation…
The ADN4695 has an input compliance range of -1V to +3.4V which is likely exceeded in your setup.
It also is way faster than what you need at 100Mbps so any spikes will make it through to the processor.
You should either use RS485 type transceivers…
LTM2894
|
LTM2895 |
LTM9100 |
LTM2885 |
LTM2881 |
LTM2882 |
LTM2883 |
LTM2884 |
LTM2893 |
LTM2886 |
LTM2887 |
LTM2889 |
LTM2892 |
LTC1694-1 |
LTC4300 |
LTC4310 |
LTC4302 |
LTC4305 |
LTC4304 |
LTC4303 |
LTC4306 |
LTC4307 |
LTC4307-1 |
LTC430… |