• ADN4680E Part-to-part Skew Repeatability

    The ADN4680E M-LVDS transceiver has a fairly-large level of part-to-part skew, but the data sheet does not have a lot of detail on what factors contribute to this. Should I expect these shifts to be largely static, from manufacturing, and thus calibratable…

  • About connection between ADN4680E and FPGA

    Hi all,

    We are considering the following configurations using ADN4680E.

    We want a direct connection between the ADN4680E and the FPGA.
    Is this method correct?
    Or should we also use a Buffer IC or something like that?

    If there are any problems, it would…

  • RE: ADN4662/ADN4664 High-Z O/P's on Powerdown

    Apologies, yes, ADN4662 and ADN4664 are LVDS receivers so it's the CMOS outputs that are being referred to here; they will be high impedance when the part is powered off.

    Another option if you prefer would be to use our MLVDS transceivers, as these…

  • 官方资料上线丨《数字隔离和接口技术选型指南2021》免费下载ing~

    “数字化”正在全球范围内掀起浪潮,推动科技如闪电般速度发展:数字医疗健康、电动汽车、 5G通信和智能制造……
    电子化器件中离不开隔离技术,而数字隔离凭借其更低的噪声和电磁干扰、更高的安全性以及更长的使用寿命,是隔离发展的必然趋势。
    ADI在数字隔离技术方面有着丰富的经验,iCoupler数字隔离可保护人员和财产免受高压影响,并保护关键数据免受破坏性电干扰。
    那么面对不同的应用领域,如何选择适合的数字隔离和接口解决方案以最大化加速您的项目?

    AD…