• RE: strange behavior MSP430 SPI clk out to ADN4665 input

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADN4665 behavior

    Greetings,

    I am using this device to drive a "long" distance SPI bus wherein the clock, and data to read back, travel the same distance on the cable.

    The delays I measure for the signals match the expected delays per the cable mfr. spec. The…

  • ADN4665 enable inputs truth table

    Is the table 5 correct in the data sheet?

    If so, of what use is the ENABLE input?

  • FAQ: EVAL-ADIS SPI Extender

    Q:

    Do you have any reference designs that can help me extend the reach of the SPI on the EVAL-ADIS?

    A:

    ----------------------------------------------------------------------------------------------------------------------------------------------…

  • FAQ: ADIS1648x SPI Extender

    Q:

    Do you have any reference designs that can help me extend the reach of the SPI on the ADIS1648x?

    A:

    --------------------------------------------------------------------------------------------------------------------------------------------------

  • termination resistor values for daisy chained LVDS app

    I am using ADN4665 & ADN4666 to extend an SPI bus. My cables are twisted pair. I have 100 ohm termination resistors on each board of which there can be a total of 4 daisy chained. Three run fine. When I add the 4th I have weird things happening to my…

  • TAGS LIST: Interface and Isolation

    LTM2894
    LTM2895
    LTM9100
    LTM2885
    LTM2881
    LTM2882
    LTM2883
    LTM2884
    LTM2893
    LTM2886
    LTM2887
    LTM2889
    LTM2892
    LTC1694-1
    LTC4300
    LTC4310
    LTC4302
    LTC4305
    LTC4304
    LTC4303
    LTC4306
    LTC4307
    LTC4307-1
    LTC430…
  • any solution for lvds driver from FPGA

    I use cyclone FPGA to get lvds signals. The project need drive lvds for a long distance . I find ADN4665 and ADN4666 ,but I can not find the clock driver . Can anybody give me some sugestions?

  • RE: TFT-Monitor Interface: VGA / DVI In, LVDS out

    I'd look at HDMI Display Interfaces at

    http://www.analog.com/en/audiovideo-products/analoghdmidvi-interfaces/products/index.html

    These only have single ended outputs, if you need true LVDS signalling then you'll need to use a LVDS driver such as…

  • 官方资料上线丨《数字隔离和接口技术选型指南2021》免费下载ing~

    “数字化”正在全球范围内掀起浪潮,推动科技如闪电般速度发展:数字医疗健康、电动汽车、 5G通信和智能制造……
    电子化器件中离不开隔离技术,而数字隔离凭借其更低的噪声和电磁干扰、更高的安全性以及更长的使用寿命,是隔离发展的必然趋势。
    ADI在数字隔离技术方面有着丰富的经验,iCoupler数字隔离可保护人员和财产免受高压影响,并保护关键数据免受破坏性电干扰。
    那么面对不同的应用领域,如何选择适合的数字隔离和接口解决方案以最大化加速您的项目?

    AD…