Termination at the input with 100 ohms will be sufficient for ADN4655 and ADN4656. ADN4654 doesn't have the terminated failsafe built-in, so external biasing would be required (pull-up on D+, pull-down on D- to ensure >100 mV for logic 1).
ADN4655…
Termination at the input with 100 ohms will be sufficient for ADN4655 and ADN4656. ADN4654 doesn't have the terminated failsafe built-in, so external biasing would be required (pull-up on D+, pull-down on D- to ensure >100 mV for logic 1).
ADN4655…
Various reports indicate that the digital isolation market will grow at over 6% per year, for the next 5 years. This growth coupled with faster communication speeds, in excess of 1Gbps, is reshaping many markets and applications. In this webcast,… |
AD…