Hi ADI Teams
Can you check the Voc( VOH/ VOL) range when there is no input signal( DINx no connected) . We test the Voc is about 2.2V using multimeter when VDDx power on. The figure 18 /19 in data sheet is lower than 2.2V.
Hi ADI Teams
Can you check the Voc( VOH/ VOL) range when there is no input signal( DINx no connected) . We test the Voc is about 2.2V using multimeter when VDDx power on. The figure 18 /19 in data sheet is lower than 2.2V.
Hello,
I am using the ADN4654 to isolate MIPI CSI-2 (High speed only) and believe the ADN4654 inputs are compatible but the ADN4654 outputs require AC caps to remove the DC offset for the MIPI receiver.
My circuit is:
DS90UB960-Q1 --> ADN4654 (100 ohm…
Whats your suggestion after ADN4653? Would that work with normaly MIPI DPHY receiver directly?
Hi sir, i am Rohanth
since this is adn4654 is not working for mipi csi2 isolation then what will the alternative ic or solution without converting to any other video format standards.
Hi ADI Expert,
My customer would like to implement the LVDS isolator ADN4654/5 in the DisplayPort, May I have your confirm for this application is workable? Thanks.
Best regards.
Ray.
It is posible to invert LVDS inputs in a ADN4654 isolator?
We have a LVDS outup form ADC and, because of pcb routing issues, it would be desirable to connect the Positive LVDS output to negative input in ADN4654 an the Negative LVDS output to positive…
Hi
Please support ADN4654 for MIPI signal issue. Thank you
Q1.Is it normal that Isolator input -data (ADN4654 DOUT2) has a coupling waveform?
Q2.How to solve the problem of abnormal DATA waveform (possibly CLK coupling)?
Q3.When measuring DOUT2, will…
Hello.
We need to implement galvanic isolation in video equipment with VGA, CVBS and DVI input interfaces.
The following diagram shows one of our approaches.
Although the input image may be at 1920x1080p60 (Full HD), it will be converted to 1280x720p60…
Hello.
In the ADN4654 data sheet, on page 3, there is a 80mA (max) supply current specification.
I'm not sure if this value is defined for each of the isolated power domains or if it is a total current consumption of the device.
In the first case…