1. LOS IRQ can only be supported to 1.8V
2. VTTI supply range = 1.8V (+/-10% tolerance)
3. VTTO supply range = 1.8V to 3.3V (+/-10% tolerance)
1. LOS IRQ can only be supported to 1.8V
2. VTTI supply range = 1.8V (+/-10% tolerance)
3. VTTO supply range = 1.8V to 3.3V (+/-10% tolerance)
Hello,
We plan to use ADN4612 as a 3G-SDI cross point switch with 75 ohm termination cable. I found that 50 ohm internal termination available at source and destination end inside the chip.Does it create any wave effect when i connect standard 75 ohm…
Hi ,
I notice that this query has been unanswered for some time. is this still an issue for you?
Regards,
David
Hello,
We plan to use ADN4612 as a 3G-SDI cross point switch with 75 ohm impedance cable. I found that 50 ohm internal termination available at source and destination end inside ADN4612. Does it create any wave effect/signal loss when i connect standard…
The device is described as protocol agnostic but I would like someone to confirm if it supports 8b/10b. The datasheet specifies 64b/66b. If it does support 8b/10b please specify the maximum speed. The device will be used to switch between Serdes…
Config time (via EEPROM) for the ADN4612?
Hi Everybody!
Can you send me IBIS or IBIS-AMI for ADN4612 ?
Thanks a lot.
Best Regads,
Viktor
vik1228@sch.bme.hu
Can I use AD8156 and ADN4612 in HDMI 2.0 applications. They want to know whether these switches will work with HDMI 2.0 protocol. Thread 36599 on ADI’s Engineer Zone states “The ADN4612 is an asynchronous, protocol agnostic crosspoint switch, which means…
I have a question regarding the ADN4612,
I am interested in using it with an LVDS signal at a rate of about 1 Gbps. There does not seem to be any information in the datasheet that would suggest there would be any wrong with this, I would just like to…
Hello,
I am looking at the ADN4612 and I was wondering how the part behaves with a pathological signal applied to it (i.e. 0x300 followed by 0x198 to give you 19 zeros followed by a unique one or vice versa). I would be interested to know how the equalizer…