各位专家好,我是研一的学生,老师最近让我看ADN2915的评估板,就是想对采样的10G信号或量化不够好的10G信号更好的量化,希望能出现规则的好的0、1码型,可一直没看懂评估板应该怎样使用的!
提供手动或自动限幅调整和手动采样相位调整。此外,用户还可选择在输入端连接一个限幅放大器或均衡
器。均衡器为自适应或可手动设置。可选限幅放大器和均衡器输入?适用于8.5 Gbps到11.3 Gbps的数据速率。前端可配置用来将不归零(NRZ)输入波形放大或均衡到满量程数字电平?
不懂这些功能这些功能怎样实现的…
I am using the ADN2917 differential output as single ended inputs into the HMC856 and HMC726. The system is communicating at 10Gbps. I don't have the option of using a clock buffer. Can the circuit be connect like below?
AD800 |
AD803 |
AD807 |
AD808 |
ADN2804 |
ADN2805 |
ADN2806 |
ADN2807 |
ADN2811 |
ADN2812 |
ADN2813 |
ADN2814 |
ADN2815 |
ADN2816 |
ADN2817 |
ADN2818 |
ADN2819 |
ADN2855 |
ADN2905 |
ADN2913 |
ADN2915 |
ADN2917 |
ADL5315 |
ADL5317 |
LTC5100 |
So far, we have been using ADN2915 and ADN2017 for clock and data recovery, however, all of these chips are not available now, and we just examined 2905, which is data recovery IC.
In the datasheet of ADN2905, all of ADN2905, 15, 17 have pin combatibility…
Hi Sir,
Due ti we saw on the website that the CDR(ADN2905/15/17) has been NRND.
May I know ADI have new part for instead ? Thanks!
The user guide tells you how to use it as a PRBS generator or checker but not both. Is there a way to simultaneously use both functions. My goal is to use it as a Bit Error rate tester - generates a PRBS stream to send through a channel and check if the…