• ADN2880: MAX leakage current specification of ADN2880 input

    Do you have the MAX leakage current specification of ADN2880 input(PIN2)?

     

    ADN2880 is one of our high speed TIA device. Pin 2 is the photo-diode current
    input pin.
    In fact, all of the TIA specs are in the datasheet table one.

    Usually…
  • Question for ADN2880

    Hello,

    I have some questions for ADN2880 from customer.

    Q1)

    Pad 4 and Pad 5 are described to connect to cathode of photo diode but the PD which the customer use can bonded just single wire. The customer would like to know which pad they should use…

  • ADN2880 for phase measurement


    My application is precise optical phase measurement.

    I am curious if there would be a phase shift as the output voltage from ADN2880 approaches to or goes over the maximum differential swing which is 260mVp-p.

    Can you also provide me the estimated values…

  • ADN2880

    We want to use ADN2880 in laser communication system at data rate 155 Mbps (STM-1). Will it support this low data rate or there is any minimum data rate limit?

  • ADN2880 gain at 1,5GHz

    Good evening:

    We're looking to use the ADN2880 for a Free Space Comunications system. The signal received is at 1,5GHz, and the PIN photodiode has a capacitance of 1,25pF. This provides a max. transimpedance resistor of 106ohm, but the ADN2880 has a…

  • SFP-RDK : ROSA, TOSA LED - source & schematic of SFP-RDK

    Can I get source & schematic of SFP-RDK?

     

    Yes, please see attached the schematic for one of SFP module reference designs.
    Please note, the ADN2870 can be replaced with ADN2872 to get better performance.

    The SFP-RDK includes:
    - SFP Transceiver…

  • Is logarithmic RF detector ADL5513 a fully differential design ?

    Hello

    I have a question regarding the logarithmic RF detector ADL5513. In the datasheet
    (www.analog.com/.../ADL5513.pdf) on page 13 is written that it is a fully
    differential design but on page 14 under section INPUT SIGNAL COUPLING is written : “The RF…
  • RE: ADN2820 Question

    Dear Caros976,

    Have you tried your photo-diode with ADN2820 yet?

    In fact, ADN2880 might be a better TIA candidate for the target application data rate range: " 1.4 GHz and 2.6 GHz (the data will have about 2 Gbits/s). "

    ADN2880 could be bonded…

  • 2 GHz - low noise - TIA

    Hello,

    I am looking for a high-bandwidth opamp (or transimpedance amplifier) for an application with the following requirements:

    - bandwidth greater than 1.5-2 GHz;

    - optical sensitivity greater than -33-35 dBm to be able to detect signals of 0.1uA;

  • TAGS LIST: Optical

    AD800
    AD803
    AD807
    AD808
    ADN2804
    ADN2805
    ADN2806
    ADN2807
    ADN2811
    ADN2812
    ADN2813
    ADN2814
    ADN2815
    ADN2816
    ADN2817
    ADN2818
    ADN2819
    ADN2855
    ADN2905
    ADN2913
    ADN2915
    ADN2917
    ADL5315
    ADL5317
    LTC5100