• ADN2817 error correction

    My receiver signal may have some "errors" introduced due to  various factors
    Can the ADN2817 be able to remove and "clean up the signal". 

    Hence Can the CDR remove errors  seen on its inputs so that its output is
    effectively…
  • New chip equivalent to ADN2817

    I want to make a clock and data recovery circuit for a plastic optic fiber link NRZ data @10Mbps to 100Mbps (different data rate for different links 10, 50 and 100 Mbps). Can you please suggest any chip please?

    I found that adn2817/2818 is not recommended…

  • Output timing of ADN2817 CDR chip

    I'm designing a board with eight ADN2817 CDR chips. Trying to determine the expected output timing (clock to data) of the CML outputs. References to the data sheet.

    Figure 2 on page 8 shows the clock and data, and labels a setup time and hold time…

  • RE: If ADN4612 can both support 1.25G 2.5G and 10G ?

    Sorry for the delay.  Evaluation board materials have been sent offline.

    We recommend the ADN2817  or ADN2818 as "recommended/preferred" instead of ADN2812.  ADN2817/8 are newer products.

  • RE: ADN2814 and Hotlink?

    Dear Dave,

    ADN2817 is one any rate CDR, which supports from 10Mbps upto 2.7Gbps, continuous mode (NRZ type, PRBS) data inputs.

    In ADN2817 family, if you are interested in the 167Mbps data link only, you might think about a cost down derivative: ADN2816…

  • What is the latency through the ADN28XX and 29XX devices?

    I'm looking at a few of the CDR chips and I don't see anything on the input to output delay through the chip.  Do you have any information on the latency for the ADN28XX series or ADN29XX series.  Specifically I'm looking at the ADN2817 and the…

  • TAGS LIST: Optical

    AD800
    AD803
    AD807
    AD808
    ADN2804
    ADN2805
    ADN2806
    ADN2807
    ADN2811
    ADN2812
    ADN2813
    ADN2814
    ADN2815
    ADN2816
    ADN2817
    ADN2818
    ADN2819
    ADN2855
    ADN2905
    ADN2913
    ADN2915
    ADN2917
    ADL5315
    ADL5317
    LTC5100