• ADN2526 and ADN2531 evaluation boards

    Dear All,

    I am a happy user of EVAL-ADN2525 evaluation board. I am considering a purchase of new evaluation boards and unfortunately, I cannot find specification sheets of these boards on Analog web site.

    Can you help me to gather more information please…

  • Evaluation Boards for the ADN2531

    How could a University order the EVAL Boards for the ADN2531?
    Nothing in stock and it says “contact ADI”

     

    In general, we do not offer “free bean” samples now. You might need to talk to
    Doug and get his approval for a loaner board.
  • ADN2531: Can output be configured as current source?

    Could the output of the AN2531 (IMODP, IMODN)be treated as current source
    meaning the output current from IMODP(N) is totally independent from the load
    and is adjusted with the MSET pin?

     

    All of our 10G, direct modulated laser diode…
  • ADN2531

    Hi, 

    We try to convert USB 3.1 to optical communication.(application: 'USB 3.1 Active Optical Cable')

    Can I use 'Laser driver(ADN2531)' to convert USB 3.1 to optical?

    Is it possible to configure it as follows?

       USB Host --<Laser Driver…

  • 5GHz (or more) VCSEL Linear Driver for High Modulation Formats

    Hello Team,

    My application require to drive VCSEL with high modulation format (e.g. PAM-4, 5GBps = 10 Gpbs). Hence, I need a linear laser driver to modulate the VCSEL with several level of power outputs.

    Can ADN2531 support such modulation formats? If…

  • RE: Need your help for choosing Laser Driver Device

    Dear Se-woong,

    Thank you for being interested in Analog Devices products.

    ADN2531 is one of quantizer type of laser diode drivers. It supports directly modulated laser by sinking bias and modulation currents from a DML laser diode. Please note, with…

  • TAGS LIST: Optical

    AD800
    AD803
    AD807
    AD808
    ADN2804
    ADN2805
    ADN2806
    ADN2807
    ADN2811
    ADN2812
    ADN2813
    ADN2814
    ADN2815
    ADN2816
    ADN2817
    ADN2818
    ADN2819
    ADN2855
    ADN2905
    ADN2913
    ADN2915
    ADN2917
    ADL5315
    ADL5317
    LTC5100
  • 1550 nm VCSEL driver

    Hello,

    I am looking for a driver for direct-modulation of a 1550 nm VCSEL (Cylindrical TO package, manufactured by Raycan).
    I noticed AD product: ADN2531 and its evaluation boards: EVAL-ADN2531-NPZ , EVAL-ADN2531-NTZ.

    I have the following questions…