• ADN2526 and ADN2531 evaluation boards

    Dear All,

    I am a happy user of EVAL-ADN2525 evaluation board. I am considering a purchase of new evaluation boards and unfortunately, I cannot find specification sheets of these boards on Analog web site.

    Can you help me to gather more information please…

  • RE: ADN2526 need propagation delay spec, please...

    Dear Mathew,

    ADN2526 is designed to support continuous mode data stream. ADN2526 coverts the modulation voltage input signal to the IMOD current signal.

    Because the low signal bit error rate is the ultimate design goal for continuous mode telecomm and…

  • RE: ADN-2530_VCSEL_Driver_Linearity_Inquiries

    Dear Meghlok,

    ADN2526 uses the similar design as that of ADN2530.

    ADN2526 is good at supporting FP or DFB direct modulated lasers,

    and provides wider bias and swing current operation ranges.

    So ADN2526 should behave the same way as that of ADN2530…

  • RE: LVPECL swing converter

    Dear Mathew,

    ADN2526 takes a differential voltage modulation input in CML logic, converts this voltage signal to a modulated current sink signal with an internal 50 ohm termination. With a matched load (<50ohm), the max. Imodp/Imodn (compliance) voltage…

  • ADN2531: Can output be configured as current source?

    Could the output of the AN2531 (IMODP, IMODN)be treated as current source
    meaning the output current from IMODP(N) is totally independent from the load
    and is adjusted with the MSET pin?

     

    All of our 10G, direct modulated laser diode…
  • TAGS LIST: Optical

    AD800
    AD803
    AD807
    AD808
    ADN2804
    ADN2805
    ADN2806
    ADN2807
    ADN2811
    ADN2812
    ADN2813
    ADN2814
    ADN2815
    ADN2816
    ADN2817
    ADN2818
    ADN2819
    ADN2855
    ADN2905
    ADN2913
    ADN2915
    ADN2917
    ADL5315
    ADL5317
    LTC5100