• ADMV8818 Process

    Hello, 

    I'm wondering if you can tell me the process (CMOS, BiCMOS, GaAs, ect) for this part?

    Thank you

  • RE: ADMV8818 setup confusion

    Please see the responses below:

    1. There are 5 write register groupings.  If more than one is active, the lower value of x for WRx_SW/FILTER is the one that is chosen.
      1. This is true when using the SPI streaming transaction.
      2. If SPI streaming is not used,…
  • RE: ADMV8818 SPI Questions

    Hi Işıl,

    Apologies for the delayed response. Here's some information:

    • Yes, the device is normally configured for MSB first. Regarding clock polarity, the SDI data is clocked through on the SCLK rising edge.
    • The SDO pin is high-Z when not in use and…
  • RE: ADMV8818 DIGITAL TUNABLE BPF S PARAMETER FILE

    Hello, 

    May I also get a link to the s-parameter files that are available for the ADMV8818? Thanks.

  • RE: usage of HMC892A

    Hi Ma Yugang,

    Apologies for the delayed response on this inquiry, as I missed during the holiday season. Yes, the HMC892A insertion loss can vary from -13 to -7dB depending upon the frequency of operation. Typically these tunable filters are placed after…