• ADMV7310 footprint

    Hi!

    Besides the distance (0.208'') there is another small difference between footprints in the datasheet and from BXL-file in the area of connection GND-pads:

     - in the DS - main polygon GND is connected to all GND-pads:

    - from the BXL-file there…

  • ADMV7310 footprint discrepancy

    Hi!

    Footprints for ADMV7310 provided in the datasheet and derived from BXL file differ - namely, the distance between the "center" and the vertical side of waveguide is 0.208" according to the datasheet and it is 0.2115" in the BXL file.…

  • RE: 36GHz RF oscillation signal source

    You need a PLL which drives a frequency doubler which drives an amplifier. Possible choices might be ADF4371 (PLL),  HMC1105 (frequency doubler) and HMC7229 (amplifier). These are not the only choices.

      PDF