• Is ADMV4801 Silicon On Insulator

    Hi EZ,

    Is ADMV4801 Silicon On Insulator?

    If not, can ADI customize it?

  • ADMV4801 RX NF test condition?

    Hi all,

    @ ADMV4801 RevSp0 datasheet, about Noise Figure spec.,

    6 page  Table.3

    Receiver Noise Figure 17 dB (typ)

    24 page  RECEIVER MODE

    Figure 61 ~ 63

    Q1

    Are these two measurement conditions the same?

    Single Receiver channel to RF ?

    Q2

    How to caluculate…

  • ADMV4801 multichip synchronization

    Would I be able to create a 32-element phased array by using two ADMV4801 chips and synchronizing them or does the chipset not have that capability?

  • How to supply the power to the ADMV4801 EVALZ board?

    Hello. I'm Junyeol Hong, a research member in Hanyang Univ. Korea.

    We already has a NDA in place, and received SPI note with purchasing 3 of your evaluation boards.

    But it doesn't have any information about the DC power that should be supplied into…

  • Are evaluation software and source code for ADMV4801 evaluation board available?

     Hello, I recently purchased ADMV4801 evaluation board. However, I could not find the evaluation software since it is pre-release.

     Can you provide ADMV4801 evaluation software and its source code if it is available? When I was using ADAR1000 evaluation…

  • Are evaluation software and source code for ADMV4801 evaluation board available?

     Hello, I recently purchased ADMV4801 evaluation board. However, I could not find the evaluation software since it is pre-release.

     Can you provide ADMV4801 evaluation software and its source code if it is available? When I was using ADAR1000 evaluation…

  • 你知道这大半年ADI都发生了哪些大事儿?

    转眼就是九月了呀,2019的大半年已经过去啦,这段时间里咱ADI可没有闲着哟~今天斑竹给大家盘点下这大半年ADI都发生了哪些大事儿吧~

    ADI与Momenta合力加速自动驾驶高精度地图产业化

    2019年1月4日,ADI 宣布与 Momenta 联合宣布达成战略合作,双方在自动驾驶高精度地图领域展开紧密合作,共同推动自动驾驶安全落地。高精度地图能够为自动驾驶车辆提供准确、实时的信息,保障安全行驶,是实现自动驾驶不可或缺的一环。ADI与Momenta的首期合作已围绕高精度地图的建图与更新相关技术展开…

  • RE: 36GHz RF oscillation signal source

    You need a PLL which drives a frequency doubler which drives an amplifier. Possible choices might be ADF4371 (PLL),  HMC1105 (frequency doubler) and HMC7229 (amplifier). These are not the only choices.

      PDF