• ADMV4530 readback

    Hi,

    I'm trying to read back register contents from the admv4530 chip and the waveform from the SDO is flat.
    I know the register writes are working as I played around with the MUXOUT making it logic high etc.

    Here is the pseudo code for the operations…

  • ADMV4530 SPI MISO held high

    Hi Experts:

    We are trying config through SPI and meet MISO issue. Below photo are the waveform of LSB first W/R Reg #0, but MISO level always high. (Same result with MSB first)

    Could you please advise why MISO pin always high? 

    Thanks in advance!

  • A Couple of Questions about ADMV4530

    Hello,

    I've not seen anything in the DS to clerify:

    • Can the reference be different from the 200MHz specified, if so, what are the Min and Max values?
    • What is the minimal level for the Ref_In power for operation? Only AMR voltage levels are specified…
  • 问几个关于admv4530的问题

    关于admv4530有几个问题想咨询下专家:

    1,admv4530的参考输入是否可以使用200M的晶振

    2,我的理解是admv4530是一个单芯片上变频器解决方案,看功能框图,RFOUT在输出时进行了两次放大,增益50db,RF增益和中频增益可调范围70dbm。这是不是意味着如果用admv4530设计上变频器,在输出后可以不用再进行滤波放大,信号直接给omt和馈源上星。

    3,admv4530的IF输入范围是2G-3G,那如果调制解调器的中频信号范围是1850M-2300M,如何调整admv4530的IF输入…

  • 问几个关于admv4530的问题

    关于admv4530有几个问题想咨询下专家:

    1,admv4530的参考输入是否可以使用200M的晶振

    2,我的理解是admv4530是一个单芯片上变频器解决方案,看功能框图,RFOUT在输出时进行了两次放大,增益50db,RF增益和中频增益可调范围70dbm。这是不是意味着如果用admv4530设计上变频器,在输出后可以不用再进行滤波放大,信号直接给omt和馈源上星。

    3,admv4530的IF输入范围是2G-3G,那如果调制解调器的中频信号范围是1850M-2300M,如何调整admv4530的IF输入…

  • 问几个关于admv4530的问题

    关于admv4530有几个问题想咨询下专家:

    1,admv4530的参考输入是否可以使用200M的晶振

    2,我的理解是admv4530是一个单芯片上变频器解决方案,看功能框图,RFOUT在输出时进行了两次放大,增益50db,RF增益和中频增益可调范围70dbm。这是不是意味着如果用admv4530设计上变频器,在输出后可以不用再进行滤波放大,信号直接给omt和馈源上星。

    3,admv4530的IF输入范围是2G-3G,那如果调制解调器的中频信号范围是1850M-2300M,如何调整admv4530的IF输入…

  • 2020年 ADI 20款硬核新品,为你献上电路设计的不二之选

    你最关注的领域是什么?ADC/DAC?Power?RF?.....

    你知道ADI在这些领域都推出了怎样的硬核新品吗?

    回首2020年,虽然被疫情干扰,不过咱ADI依旧没有停止推出新产品的脚步,今天斑竹就为大家盘点一下今年的“新秀”吧~

    四通道、软件可配置输入/输出 AD74412R/13R

    AD74412R 是一款适用于楼宇和过程控制应用的四通道软件可配置输入/输出解决方案。AD74412R 包含用于模拟输出、模拟输入、数字输入和电阻温度检测器 (RTD) 测量的功能,这些功能集成在一个单芯片解决方案中…

  • ADI 全新中文资料(2019 年 6 月)

  • 3-4月ADI新品主打,快来康康有没有适合你的设计~

    携一缕浅夏的芬芳,凝一脂冰清玉洁的清梦

    各位小伙伴们,迷人的仲夏五月来啦~

    在这个似水的季节里,悠然翻阅学习岂不美哉?

    今天斑竹给大家带来 ADI 3 - 4月的新品合集,想要了解学习的筒子可千万不能错过哦~

    MxFETM四通道 16 位 12GSPS RFDAC 和双通道 12 位 6GSPS RFADC AD9082

    发射信号前端 (MxFE®) 是一款高度集成的器件,具有 16 位、12 GSPS 最大采样率射频 (RF) 数模转换器 (DAC) 内核和 12 位、6 GSPS 采样率…

  • 在新年到来之际,送你一组钻石级硬度的精选硬核产品吧~

    转眼间,2020年就要结束了,今年你都做了些什么呢?

    对于ADI,我们可是推出了不少硬核产品哦~

    今天,斑竹就给大家晒晒ADI这些杠杠滴成果!

    -------------------------------------------------------------------------

    软件可配置的四通道输入/输出 AD74413R

    AD74413R是一款软件可配置的四通道输入/输出解决方案,适用于楼宇和过程控制应用。AD74413R包含用于模拟输出、模拟输入、数字输入、电阻温度检测器(RTD…